Sie befinden sich auf der alten Website von www.rittal.de Zur neuen Webseite von Rittal
Wishlist

Press releases

Image source: Deutsche Messe

Rittal at the Hanover Fair 2013

2013-04-08. Friedhelm Loh took to the stage with German Chancellor Angela Merkel and Russian President Vladimir Putin to officially open this year’s Hanover Fair (Hannover Messe).

Read article!
  • International partnership offers great marketing platform

    2014-03-12. Rittal entered a worldwide partnership agreement with DatacenterDynamics (DCD), London, in the field of marketing. As a result, the provider of IT infrastructure has been granted international access to the services of DatacenterDynamics, allowing Rittal to present its data centre portfolio to a larger audience.

  • Energy-efficiency in a package

    2014-02-11. The PUE efficiency package for the RiMatrix S standardized data centre solution is now available at last. This means Rittal is offering its customers an optional package of hardware and software that gives IT administrators information on efficiency values in the data centre quickly and simply.

  • Rapid mounting system for flat screens

    2014-02-07. Panel PCs and TFT screens, suitable for industrial applications, are increasingly being used by operators to control plant and machinery. Rittal has developed the new VESA 75/100 connection console, so these devices can be mounted to the CP 40/60/120 support arm system quickly and easily.

  • Industrial protection for office monitors

    2014-01-29. Increasingly, plant engineering companies are using conventional office TFT screens in their operation solutions for plant and machinery. Rittal housings for desktop TFT screens offer outstanding protection and an attractive design.

  • Automatic potential equalisation closes safety gap

    2014-01-15. Safety first – this also applies in the installation of support arm systems for machine operation. Rittal has closed a dangerous security gap at the human-machine interface through an automatic potential equalisation of its new CP 60/120/180 support arm system.

  • What you need to know about cooling technology

    2013-12-19. With good advice, valuable tips and solutions, the Rittal technology library exists to help users from industry and IT. Now, the second volume "Enclosure and process cooling" has appeared.

  • RiMatrix S comes to Middle Earth

    2013-12-05. Rittal, a provider of end-to-end IT infrastructure solutions, has received its first international order for its standardised data centre, RiMatrix S. The customer, Orion, is a New Zealand based utility that will use the data centre to deliver a more stable power supply to the residents of Christchurch.

  • Seven steps to your own data centre

    2013-11-28. Up to now, several months were needed to design and build a data centre. That can now all be done much faster with RiMatrix S, the modular, standardised data centre from Rittal.

  • The new Rittal catalogue has arrived!

    2013-11-06. A print run of 220,000, 20 different languages, 744 pages – these are the impressive figures on the new 2014/2015 Rittal Catalogue. With the product catalogue, the company wants to inform the international industry and IT markets about its complete series system program even faster and better.

  • Refrigeration machines that fit perfectly are now available

    2013-08-15. The requirement profiles for the use of recooling systems (chillers) are varied. To respond even more strongly to the needs of individual industrial sectors, primarily for engineering and increased availability, Rittal has developed a new generation of its TopTherm chillers in the 8 to 40kW output categories.